Synergy Devices Limited - SpeedMixer™

System Mixing PotSpeedMixer.co.uk
SpeedMiixer


See us at MEDTEC UK 2008 - 13th to 14th February 2008 - more details...

Below Header
UK Site
Home Page Company Products News and Events Contact us Login
Below Header
DAC 150 Series
DAC 400 Mixers
DAC 600 Mixers
DAC 800 Mixers
DAC 1100 Mixers
DAC 3000 Mixers
Containers
Dispensing Equipment
Mixing Service
Microscopy SEM Service 
Resources

A National and International service supplying the SpeedMixer™ by Hauschild.
Supporting a full range of Mixing and Dispensing Products.

See our international sales page
International sales...


 

 

 

 

 

 

 

 

 

 

SpeedMixer™ Product Range

DAC 800 FVZ DAC 3000

All the DAC Range of SpeedMixers use disposable Jars and Lids. These eliminate clean up and have the added advantage of enabling the user to store material once mixed.

Sizes Max 10 – Max 300 Containers are available along with their corresponding Holders, dependent upon the model of machine. Sample mixes of 3g to 300g can be achieved.

 

The DAC 400 Series and the DAC 150 FVZ-K & FV-K mixers have the capability to take Syringes and Cartridges in an appropriate holder. The operators can then pre mix in the barrel and, as once mixed the material can be dispensed directly, it eliminates the need for down packing.

 

Multi Holders are available for the 400 Series to enable the operator to use an extremely wide range of containers, syringes and cartridges allowing for several samples to be mixed at the same time.

 

Some of the containers used across the product range

Containers

All the DAC Range of SpeedMixers use disposable Jars and Lids. These eliminate clean up and have the added advantage of enabling the user to store material once mixed

 

 

 

 

Dispensing

We can supply dispensing equipment from Manual Dispensing Guns to Tailor Made Dispensing Machines. We hold a comprehensive range of Hybrid Syringe Systems with sizes from 5cc to 30cc
We have the answer to almost every requirement due to the diversity of our range.

 

 

Back to top