Synergy Devices Limited - SpeedMixer™

System Mixing PotSpeedMixer.co.uk
SpeedMixer


more details...

Below Header
UK Site
Home Page Company Products News and Events Contact us Login
Below Header
Dac 150 Mixer Range
Dac 400 Mixer
Dac 600 Mixer
Dac 800 Mixer 
Dac 1100 Mixer
Dac 3000 Mixer
Containers
Cups & Holders - 150
Cups & Holders - 400
Dispensing Equipment
Mixing Service
Resources

A National and International service supplying the SpeedMixer™ by Hauschild.
Supporting a full range of Mixing and Dispensing Products.

See our international sales page
International sales...


 

 

 

 

 

 

 

 

 

 

Containers & Holders

All the DAC Range of SpeedMixers use disposable Jars and Lids. These eliminate clean up and have the added advantage of enabling the user to store material once mixed.

 

Sizes Max 10 – Max 300 Containers are available along with their corresponding Holders, dependent upon the model of machine. Sample mixes of 3g to 300g can be achieved.

 

The DAC 400 Series and the DAC 150 FVZ-K & FV-K mixers have the capability to take Syringes and Cartridges in an appropriate holder. The operators can then pre mix in the barrel and, as once mixed the material can be dispensed directly, it eliminates the need for down packing.

 

Multi Holders are available for the 400 Series to enable the operator to use an extremely wide range of containers, syringes and cartridges allowing for several samples to be mixed at the same time.
Placeholder Image

 

 

 

Mixing System

All the DAC Range of SpeedMixers use disposable Jars and Lids. These eliminate clean up and have the added advantage of enabling the user to store material once mixed.

Placeholder Image

 

Back to top